SYSTIMAX® Solutions Launches New Connectivity Solution for Harsh Environments

Cabling Protection from Harsh Environments Now Available
14. September 2005 RICHARDSON, Texas

SYSTIMAX® Solutions, the worldwide leader in structured connectivity solutions, today announced the availability of a connectivity solution for harsh environments such as pharmaceutical and automobile manufacturing plants. The solution is compatible with the current SYSTIMAX® product range and is IP65 and IP67 rated to protect cabling from water and dust ingress at temperatures between -13ºF and 185ºF (-25oC and 85oC). The International Protection (IP) rating system classifies the degree of protection from solid objects and liquids afforded by electrical equipment and enclosures.

The SYSTIMAX Ruggedized Connector System has a corrosive-resistant, gasketed faceplate to protect the cable and connectors from the harsh surrounding environment. The solution also has built-in features to prevent accidental disconnections and rotation when mounted to the faceplate.

“We work with the world’s top manufacturing and industrial companies who need to be confident that their connectivity solutions are protected from the everyday strain of industrial use,” said Joseph Storey, SYSTIMAX Copper Apparatus Product Manager. “The risks regularly include harsh temperatures and humidity along with exposure to water and dust particles. Our new solution protects against these situations while complimenting our product range by offering ease of installation and administration.”

The solution is now available globally and more information on the solution can be found at www.systimax.comor at your local SYSTIMAX Solutions office.

About SYSTIMAX Solutions

SYSTIMAX Solutions™, a CommScope company (NYSE: CTV), is a worldwide leader in structured cabling systems and provides integrated end-to-end connectivity solutions for voice, data, video and building management applications in both wired and wireless enterprise networks.

SYSTIMAX Solutions supplies its high performance and market-leading range of products through a network of highly skilled BusinessPartners. The product range includes the copper based GigaSPEED® X10D and GigaSPEED XL Solutions, the fiber-optic LazrSPEED® and TeraSPEED™ Solutions and the intelligent patching iPatch® System. The SYSTIMAX AirSPEED™ Solution adds a wireless option to the portfolio. SYSTIMAX Labs and the people who have spearheaded these innovations will continue to play an integral role in the future success of SYSTIMAX Solutions. Currently the company’s BusinessPartners install an average of over 1,000 miles (1,600km) of SYSTIMAX cable every day in approximately 120 countries worldwide. For further information please visit http://www.systimax.com.

Forward-looking Statements

Diese Pressemitteilung enthält zukunftsgerichtete Aussagen, die auf Informationen basieren, die dem Management derzeit zur Verfügung stehen, auf den Überzeugungen des Managements sowie auf einer Reihe von Annahmen bezüglich zukünftiger Ereignisse basieren. Zukunftsgerichtete Aussagen sind keine Leistungsgarantie und unterliegen einer Reihe von Unsicherheiten und anderen Faktoren, die dazu führen könnten, dass die tatsächlichen Ergebnisse wesentlich von den derzeit erwarteten Ergebnissen abweichen. For a more detailed description of the factors that could cause such a difference, please see CommScope’s filings with the Securities and Exchange Commission. Durch die Bereitstellung zukunftsbezogener Aussagen beabsichtigt das Unternehmen nicht – und verpflichtet sich diesbezüglich in keiner Weise – diese Aussagen aufgrund neuer Informationen, zukünftiger Ereignisse oder aus anderen Gründen zu aktualisieren.

Media Enquiries:
Fiona Nolan
SYSTIMAX-Lösungen
+353 1 2042000
fnolan@systimax.com